CANOPEN.LOOPBACK

Description

This parameter allows viewing when the loopback object is updated in the drive. The loopback object can be mapped into both the Rx and Tx PDOs as a troubleshooting tool to verify fieldbus delay. The master writes the Rx Loopback (300Bh sub-index 4) and the drive should update the Tx Loopback (300Bh sub-index 3) by the next fieldbus cycle if synchronized correctly.

Context

See Synchronization.

Versions

Action Version Notes
Implemented 02-06-01-000

General Information

Type

Read Only

Units

N/A

Range

0 to 255

Default Value

N/A

Data Type

Integer

Stored in Non-Volatile Memory

No

Variants Supported

EtherCAT and CAN variants: AKD2G-SPE and AKD2G-SPC

 

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

CANOPEN.LOOPBACK

300bh

03h

Unsigned8

-

-

Read only

Yes